blhost configure-memory vs configure-quadspi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

blhost configure-memory vs configure-quadspi

1,259 Views
ernest_yeung_terran
Contributor II

For blhost, I noticed that the older version uses configure-quadspi vs. configure-memory. We are having to use the older version of blhost that has been built for the ARM architecture for https://github.com/Lauszus/blhost

* would we be able to use the blhost with configure-quadspi option in place of configure-memory and if so what input parameters would have to change if necessary?

* was there any underlying code change for configure-memory vs. configure-quadspi when blhost changed from old to new version?

* is the quadspi enumeration via flash_id the same as configure-memory enumeration for memory_id?

 

Labels (1)
0 Kudos
Reply
1 Reply

1,255 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
In my opinion, you'd better to contact the author of the variant Blhost for the ARM architecture or review the source code to check the parameters of configure-quadspi command.
Further, it's another option is using the Blhost -help command for help.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply