Hi@carlos_o
I'm sorry it took so long to get back to you.
Before, I tried to connect the interface on my board, but the error was still displayed.
Recently I got the development board of RT685. At the beginning, I used the data cable to connect J5 to the computer, and then successfully burned the program of HelloWorld. D8 and D11 on the board are in constant state, and D2 flickers.
Later, I went to check my board. The above interface is type-C, and the pins are DM and DP, and A5, B8 and VBUS, GND. I don't know why the computer is connected through the type-C port. The computer can't find any external devices, and it doesn't show the access of unknown devices.
Today, when testing the development board, I also encountered a very strange problem.
Originally, the development board was intact, and I burned the case code to enable normal burning. But when I first failed to burn my board, I changed the data line and then burned the development board, and the development board also had the initial problem of this post.
Moreover, after connecting the J5 port, only the D2 light is flashing, and D8 and D11 are not on.
Now it can't be burned in, and it always shows "unable to connect wire for probe index 1. Error: Wire Ack Fault - target connected?"
What's the reason for that? Is the board broken?