When I don't need the TX_ER output, can it be used with GPIO?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When I don't need the TX_ER output, can it be used with GPIO?

ソリューションへジャンプ
1,527件の閲覧回数
george
Senior Contributor II

Hi All,

My customer uses KSZ8081MNX with RT1170.

george_0-1693147243374.png

The KSZ8081MNX doesn't need the TX_ER signal, so my customer wants to use that pin as a GPIO.

I think that's perfectly fine, but my customer wants a comment from NXP.
Could someone please comment on that certainty?

Can the TX_ER pin be used as a GPIO?
It doesn't affect the behavior of ENET, right?

Thanks,
George

0 件の賞賛
返信
1 解決策
1,413件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @george ,

  Your understanding is totally correct!

   To the RT chip, if the pin is not used by the peripherial, it can be configured as the GPIO function.

  So, you can use it as the GPIO when you don't use it as the ENET function.

 

Wish it helps you!

If you still have question about this case, just kindly let me know.

If your question is solved, please tell me to mark the correct answer, just to close this case.

Any new issues, welcome to create the new case.

Best Regards,

Kerry

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,414件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @george ,

  Your understanding is totally correct!

   To the RT chip, if the pin is not used by the peripherial, it can be configured as the GPIO function.

  So, you can use it as the GPIO when you don't use it as the ENET function.

 

Wish it helps you!

If you still have question about this case, just kindly let me know.

If your question is solved, please tell me to mark the correct answer, just to close this case.

Any new issues, welcome to create the new case.

Best Regards,

Kerry

0 件の賞賛
返信
1,396件の閲覧回数
george
Senior Contributor II

Hello @kerryzhou,

Thanks for your comment.

BR,
George

0 件の賞賛
返信
1,393件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @george ,

  You are always welcome!

   If your question is solved, please help to mark the correct answer, just to close this case.

  Any new issues, welcome to create the new case, thanks.

Best Regards,

kerry

0 件の賞賛
返信