Use ENET_SetMII() function without disabling Ethernet MAC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use ENET_SetMII() function without disabling Ethernet MAC

2,749件の閲覧回数
ombra32
Contributor III

Hi,

I need to dynamically change MAC controller speed and duplex, based on values auto-negotiated by PHY at each link up.

In iMXRT1176 SDK there is a function named ENET_SetMII(), created exactly with that purpose:

 

/*!
 * brief Sets the ENET MII speed and duplex.
 *
 * This API is provided to dynamically change the speed and dulpex for MAC.
 *
 * param base  ENET peripheral base address.
 * param speed The speed of the RMII mode.
 * param duplex The duplex of the RMII mode.
 */
void ENET_SetMII(ENET_Type *base, enet_mii_speed_t speed, enet_mii_duplex_t duplex)
{

 

I've tried it on my code, and it works like a charm!

But iMXRT1170 Reference Manual states that TCR->FDEN register (changed by ENET_SetMII() function) can be modified only with ECR->ETHEREN = 0 (Ethernet MAC disabled).

mac2.PNG

So, now the question is: is really safe to use ENET_SetMII() function to dynamically change speed and duplex of MAC controller, without disabling it?

 

Best regards,

Marco

0 件の賞賛
返信
3 返答(返信)

2,728件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is really safe to use ENET_SetMII() function to dynamically change speed and duplex of MAC controller, without disabling it?
-- No, I'm afraid not, it's a risk to do it.
Have a great day,t
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,717件の閲覧回数
ombra32
Contributor III

Ok, so what is the best suggested way to manage ENET MAC after PHY re-link?

0 件の賞賛
返信

2,709件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) So what is the best suggested way to manage ENET MAC after PHY re-link?
-- It seems like that it needs to reInitialize the ENET module.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信