Board - iMXRT1040-EVK, SDK - mcuXpresso SDK v25.03.00, Windows, McuXpresso IDE
Hi,
I am trying to read data from the external NOR Flash on the EVK. I am using the flexspi nor edma example, but instead of using memcpy to read data I want to use "flexspi_nor_read_data()" function. Below is my code:
int main(void)
{
...
status = flexspi_nor_read_data( EXAMPLE_FLEXSP, (EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE),(void*)s_nor_read_buffer,sizeof(s_nor_read_buffer));
if (memcmp(s_nor_read_buffer, s_nor_program_buffer, sizeof(s_nor_program_buffer)) != 0)
{
PRINTF("Program data - read out data value incorrect !\r\n ");
return -1;
}
else
{
PRINTF("Program data - successfully. \r\n");
}
...
}
status_t flexspi_nor_read_data(FLEXSPI_Type *base, uint32_t startAddress, uint32_t *buffer, uint32_t length)
{
...
g_completionFlag = false;
status = FLEXSPI_TransferEDMA(base, &flexspiHandle, &flashXfer);
if (status != kStatus_Success)
{
return status;
}
/* Wait for transfer completed. */
while (!g_completionFlag)
{
}
...
}
The program goes to an infinite loop at while (!g_completionFlag) and I am getting status as 7002 as a return value from "FLEXSPI_TransferEDMA()"
I also tried the flexspi polling example, but getting the same output.
Why would the read function not work but we are able to read using memcpy?
Thanks
已解决! 转到解答。
I found the problem. I was sending incorrect address to the read function. Modified code for calling the flexspi_nor_read_data() is below.
main()
{
...
status = flexspi_nor_read_data( EXAMPLE_FLEXSPI,
(EXAMPLE_SECTOR * SECTOR_SIZE),
(void *)s_nor_read_buffer,
sizeof(s_nor_read_buffer));
...
}
Thanks
I found the problem. I was sending incorrect address to the read function. Modified code for calling the flexspi_nor_read_data() is below.
main()
{
...
status = flexspi_nor_read_data( EXAMPLE_FLEXSPI,
(EXAMPLE_SECTOR * SECTOR_SIZE),
(void *)s_nor_read_buffer,
sizeof(s_nor_read_buffer));
...
}
Thanks
By further debugging I found out when flexspi_nor_read_data() is called the EDMA IRQ Rx handler DMA1_DMA17_DriverIRQHandler() does not get called. However when reading chip ID using flexspi_nor_get_vendor_id() the DMA1_DMA17_DriverIRQHandler() is called and the read is successful. Modified flexspi_nor_get_vendor_id() is shown below. Any help is highly appreciated.
status_t flexspi_nor_get_vendor_id(FLEXSPI_Type *base, uint8_t *vendorId)
{
uint32_t temp;
flexspi_transfer_t flashXfer;
flashXfer.deviceAddress = 0;
flashXfer.port = kFLEXSPI_PortA1;
flashXfer.cmdType = kFLEXSPI_Read;
flashXfer.SeqNumber = 1;
flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_READID;
flashXfer.data = &temp;
flashXfer.dataSize = 1;
status_t status;
status = FLEXSPI_TransferEDMA(base, &flexspiHandle, &flashXfer);
if (status != kStatus_Success)
{
return status;
}
/* Wait for transfer completed. */
while (!g_completionFlag)
{
}
*vendorId = temp;
/* Do software reset or clear AHB buffer directly. */
#if defined(FSL_FEATURE_SOC_OTFAD_COUNT) && defined(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK) && \
defined(FLEXSPI_AHBCR_CLRAHBTXBUF_MASK)
base->AHBCR |= FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK;
base->AHBCR &= ~(FLEXSPI_AHBCR_CLRAHBRXBUF_MASK | FLEXSPI_AHBCR_CLRAHBTXBUF_MASK);
#else
FLEXSPI_SoftwareReset(base);
#endif
return status;
}
Thanks