USB example .inf file not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB example .inf file not working

Jump to solution
3,589 Views
lucky1408
Contributor II

Hello,

I'm trying to use the USB port as a virtual com port. I've found the example from the SDK, but when I try to install the driver which is situated in the "inf" folder I get the following error:

Virtual com port error.PNG

I've downloaded the latest SDK version, but that didn't solve the problem.

Does anybody have any experience with this?

My board is the: IMXRT1050-EVKB

With kind regards,

Luc

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,395 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Luc Aarts

Please check the following post:

NXP USB VID/PID Program  

The VID and PID are specified in the USB descriptor

Regards

Jorge Alcala

View solution in original post

0 Kudos
Reply
3 Replies
3,395 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Luc Aarts

Could you clarify what SDK example are you using? If possible please try to use another .inf file with the example that you are running. Another option is using another driver for the example.

NXP provides "demo projects" with an INF file using NXP's VID/PID. It is the customer's responsibility to get their own PID/VID and get the INF file certified by Microsoft for the end product.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply
3,395 Views
lucky1408
Contributor II

Hello jorge_a_vazquez,

I'm using SDK 2.5.1., but after using a different inf file it worked.

How do I change the VID and PID?

With kind regards,

Luc

0 Kudos
Reply
3,396 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Luc Aarts

Please check the following post:

NXP USB VID/PID Program  

The VID and PID are specified in the USB descriptor

Regards

Jorge Alcala

0 Kudos
Reply