USB booting up i.MX RT1060

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB booting up i.MX RT1060

1,068 Views
er_arpit_arora
Contributor III

Hi Yuri, pardon my lack of knowledge. I am still very new to all this. I've been reading the reference guide, data sheet and hardware development guide over the last few days.

My question is that if I connect my USB Port on my laptop and the following shown schematic, I should be able to flash i.MX RT1060?

That is the physical connection which is required is between my laptop USB port -> Micro USB socket which goes into the USB_OTG1_ID, USB_OTG1_DN & USB_OTG1_DP pins on the i.MX RT1060.

Anything else pertaining to the hardware connection for flashing purpose?

USB_OTG.png

Labels (1)
0 Kudos
Reply
1 Reply

945 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Your circuit  may be used for i.MX RT USB serial downloader mode.

I assume 5V_USB_OTG is provided by host PC on the scheme.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply