Run and read from flash at the same time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Run and read from flash at the same time

1,222 Views
rans
Senior Contributor I

Hello,

Is it possible to run from flash (hyperFlash) and read from the flash at the same time ?

For example, there is a hyperFlash demo in SDK, can it be a xip application which is reading from other parts of flash at the same time ?

Thank you,

ranran

0 Kudos
Reply
3 Replies

1,063 Views
igorpadykov
NXP Employee
NXP Employee

Hi ranran

yes it is possible to run hyperflash xip application and read from other parts of flash.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,063 Views
diogocacador
Contributor III

Is there an example application for this?

Best regards,

Diogo

0 Kudos
Reply

1,063 Views
igorpadykov
NXP Employee
NXP Employee

one can look on MCUXpresso examples

Welcome | MCUXpresso SDK Builder 

Best regards
igor

0 Kudos
Reply