USB CDC Driver Re-Certification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB CDC Driver Re-Certification

Jump to solution
1,912 Views
dh1
Contributor II

Hello

We are using CDC Class driver for our NXP RT MCU.

Now we would like to use our NXP-Assigned PID with the driver provided by NXP with the SDK. This is the fsl_ucwxp.inf file with the cdc.cat file.

First question: Is this driver certified by Microsoft?

To use this driver with our own PID, and to give a proper name in the device manager, we need to edit the .inf file. This will void the certification of the driver.
To alllow driver installation at customers without security warning, we need to re-certify the driver by Microsoft. To be able to do this, NXP will need to confirm to Microsoft that we are allowed to do this.

Is this allowed by NXP and has it been done before?

Thanks and regards,
Daniel

0 Kudos
Reply
1 Solution
1,895 Views
jingpan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
4 Replies
1,885 Views
mjbcswitzerland
Specialist V

Hi @jingpan 

Interestingly in the link that you show it points out that the NXP VID/PID program can't be used for i.MX RT parts - it is only valid for Cortex M LPC and Kinetis based products and Cortex-A based i.MX application processors.

Is that really the case?

Regards

Mark

 

0 Kudos
Reply
1,855 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @mjbcswitzerland ,

No, it can used on i.mxRT. The last update of this post is 07-15-2016. RT wasn't announced at that time.

 

Regards,

Jing

Tags (1)
0 Kudos
Reply
1,846 Views
mjbcswitzerland
Specialist V

Hi

Many thanks! That is very good to know!

Regards

Mark

 

0 Kudos
Reply
1,896 Views
jingpan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply