Troubleshooting MCUboot Utility Connection Failures

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Troubleshooting MCUboot Utility Connection Failures

1,557 Views
LHLL
Contributor I

mcubootutility connection failed. I connected the spi1_2second pins to the NOR flash (W25Q256). BT_CFG[7:0] = 4'b0000; BOOT0 = 1, BOOT1 = 0. mcupbootutility indicates it can connect to the flashloader but cannot connect to the external memory. Hardware and software configurations are as follows:Snipaste_2026-03-09_15-43-26.pngSnipaste_2026-03-09_15-44-19.pngSnipaste_2026-03-09_15-45-48.png

0 Kudos
Reply
5 Replies

1,536 Views
mayliu1
NXP Employee
NXP Employee

Hi @LHLL ,

Thank you so much for your interest in our products and for using our community.

please clarify the following information:

1: Which RT-series MCU are you using?
2: Are you working on your own custom board, or using an NXP evaluation board?
If it is a custom board, any basic hardware details would also be helpful.

Best Regards

MayLiu

0 Kudos
Reply

1,530 Views
LHLL
Contributor I

It is a custom circuit board, with the MCU using the IMXRT1166XVM5A.

0 Kudos
Reply

1,476 Views
mayliu1
NXP Employee
NXP Employee

Hi @LHLL ,

In the figure from your previous post, I wasn’t able to locate the DQS pin. Could you point out its configuration or where it is mapped?
 
Best Regards
MayLiu
0 Kudos
Reply

1,345 Views
LHLL
Contributor I

Hi MayLiu ,

I did not use the DQS pin because NOR flash does not require it. I Multiplex the DQS pin as an ETH_MDIO pin.Looking forward to your reply.

Snipaste_2026-03-12_17-22-00.pngSnipaste_2026-03-12_17-22-15.png

Best Regards

0 Kudos
Reply

1,213 Views
mayliu1
NXP Employee
NXP Employee

Hi @LHLL ,

Could you please try to set the DQS pin as floating and then test again?
 
Best Regards
MayLiu
0 Kudos
Reply