Timeout while waiting for high throughput clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Timeout while waiting for high throughput clock

跳至解决方案
4,183 次查看
emmmmmmmmmmmmmm
Contributor III

I have an RT1170 board. When I test the 4343W routine, the log prints 'Timeout While Waiting For High Throughput Clock', when starting the WiFi firmware, I want to know what the reason?
My WiFi model is 43438a1, I believe that my WiFi module is normal, I verify the function on the RT1052 board

0 项奖励
回复
1 解答
4,119 次查看
emmmmmmmmmmmmmm
Contributor III

Thank you for your reply, I have found the reason, it is the problem of my board.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
4,175 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi emmmmmmmmmmmmmm,

  Could you please tell me which detail wifi module you are using?

  From our RT1170 SDK, it has this requirement:

Hardware requirements
=====================
- 2x Micro USB cable
- MIMXRT1170-EVK board
- Personal Computer
- Murata 1DX or 1LV M.2 module
- Murata uSD M.2 Adapter
- 1 plug to receptable header cable

 

BTW, which detail SDK code you are testing?

This one:

SDK_2.9.1_MIMXRT1170-EVK\boards\evkmimxrt1170\wifi_cypress_examples\wiced_iperf_4343W

In fact, if you want to use wifi, we highly recommend you use the NXP wifi module:

SDK_2.9.1_MIMXRT1170-EVK\boards\evkmimxrt1170\wifi_examples

Hardware requirements
=====================
- Micro USB cable
- MIMXRT1170-EVK board
- Personal Computer
- One of the following WiFi modules:
- Panasonic PAN9026 SDIO ADAPTER + SD to uSD adapter
- AzureWave AW-NM191NF-uSD

 

Wish it helps you!

Best Regards,

Kerry

0 项奖励
回复
4,169 次查看
emmmmmmmmmmmmmm
Contributor III

The project I use is SDK_2.8.1_MIMXRT1170-EVK-PRC3 \ Boards \ evkmimXRT1170 \ wifi_cypress_examples \ wiced_iperf_4343w
My WiFi is NM372SM
What details do you still need?

0 项奖励
回复
4,142 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

HI @emmmmmmmmmmmmmm 

  Thanks for your updated information, your SDK version is very slow, highly suggest you download the newest SDK version:

mcuxpresso.nxp.com

BTW,  please use the project related readme.txt required WIFI module, otherwise, it may still related to your own wifi module configuration. You'd better make the original wifi project works at first, then try to modify it to match your own wifi module.

 

Best Regards,

kerry

0 项奖励
回复
4,120 次查看
emmmmmmmmmmmmmm
Contributor III

Thank you for your reply, I have found the reason, it is the problem of my board.

0 项奖励
回复