Text Formating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Text Formating

1,325件の閲覧回数
GarageDirt
Contributor II

In some of the example programs, there are lines of code that are in italics. Such as:

{kGPIO_DigitalOutput, 0, kGPIO_NoIntmode}; that is colored green.  When typing  your own code, how do you do that?  Without the code being in italics, the code does not build.

 

0 件の賞賛
返信
1 返信

1,315件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The IDE can highlight the various keywords, data types, and input/output in different ways, like bold, italic, color.
It's handled by the IDE automatically.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信