Source code for 'Application Notes'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Source code for 'Application Notes'

1,598 Views
kurt_staubli
Contributor III

Is it possible to download source code used for NXP's Application Notes? I am looking for the code for AN12214 (PMSM Field-Oriented Control on MIMXRT10xx EVK).

Labels (1)
0 Kudos
Reply
1 Reply

1,512 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Kurt,

This application does have the source code, you can download it form the following link.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply