Setting Timer in Low Power Mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Setting Timer in Low Power Mode

跳至解决方案
1,937 次查看
frozen
Contributor III

I use imxrt1176, can I set timer to wake up mcu for 24 hours ?

0 项奖励
回复
1 解答
1,919 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Yes! The first way that comes to my mind is using the GPT timer as a wakeup source, for more detail please refer to app note AN13104 Debug and Application for i:MX RT1170 Clock and Low Power Feature. If the clock and the prescaler are not slow enough, the GPT counter can be operated using an external clock (GPT_CLK) from outside the device, which in turn can be generated with another timer.

Hope it helps you.

Have a nice day!

在原帖中查看解决方案

1 回复
1,920 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Yes! The first way that comes to my mind is using the GPT timer as a wakeup source, for more detail please refer to app note AN13104 Debug and Application for i:MX RT1170 Clock and Low Power Feature. If the clock and the prescaler are not slow enough, the GPT counter can be operated using an external clock (GPT_CLK) from outside the device, which in turn can be generated with another timer.

Hope it helps you.

Have a nice day!