SDRAM Read write issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDRAM Read write issue

1,932件の閲覧回数
Adithya
Contributor I

Hi @kerryzhou


I'm trying to read and write to SDRAM with SEMC_CM7 example code, everything is working fine with EVAL board. But if i try the same thing with our customized board which is similar to Eval board, for the same SEMC FPAGA is interfaced with addition chip select.


The SDRAM chip we used in our customized board is "W9825G6KH-52344P"


With our customized board with DATALEN of 0x1000 read and write is working fine with one change in the example code (evkbmimxrt1170_semc_cm7).


1. Disabled/commented "DCACHE_InvaliddateByRange" in our code".


2. We need to go for Read from SDRAM before going for Write operation


If we increase DATALEN to 0x2000 in example code, its failing in 32/16/8 bit Read write operation. What could be the reason, Can someone help me on this.


Pls refer attached workspace.

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,848件の閲覧回数
Sam_Gao
NXP Employee
NXP Employee

Hi @Adithya 

It is strange becasue 'DCACHE_InvalidateByRange' is only for cache alignment.

Would you please help check with the below patch?

1. Set this marco to 0

// #define CACHE_MAINTAIN 0x01U
 #define CACHE_MAINTAIN 0

2. source/semc_sdram.c, add " SCB_DisableDCache()" before reading or writing.

int main(void)
{
	/* Hardware initialize. */
	BOARD_ConfigMPU();
	BOARD_InitPins();
	BOARD_BootClockRUN();
	BOARD_InitDebugConsole();

	/* Config cacheable attribute for SDRAM memory */
	APP_ConfigMPU();

#if !(defined(CACHE_MAINTAIN) && CACHE_MAINTAIN)
#if defined(__DCACHE_PRESENT) && __DCACHE_PRESENT
	if (SCB_CCR_DC_Msk == (SCB_CCR_DC_Msk & SCB->CCR))
	{
		SCB_DisableDCache();
	}
#endif
#endif

	PRINTF("\r\n SEMC SDRAM Example Start!\r\n");
	if (BOARD_InitSEMC() != kStatus_Success)
	{
		PRINTF("\r\n SEMC SDRAM Init Failed\r\n");
	}

+       SCB_DisableDCache();
	/* 32Bit data read and write. */
        SEMC_SDRAMReadWrite32Bit();
        /* 16Bit data read and write. */
        SEMC_SDRAMReadWrite16Bit();
        /* 8Bit data read and write. */
        SEMC_SDRAMReadWrite8Bit();
...
}
0 件の賞賛
返信

1,906件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Adithya ,

    Thanks so much for your trust! I already don't support the RT in the community now.

   Please don't worry, our other RT engineer will help you about your issues, please keep patient for the case reply.

Best Regards,

kerry

0 件の賞賛
返信