SDRAM ECC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDRAM ECC

Jump to solution
2,893 Views
Ootsuka
Contributor II

Hello teams.

We designed an i.MX RT1171 custom board and connect it to the SDRAM on the SEMC bus.
Please tell us how to enable ECC.

We enabled XECC_SEMC[ECC_CTRL] bit2-0 and address settings, but it doesn't work.
Must be set to the eFUSE 0x840[3] bit?
Is there any other settings ?

Best regards.

Tags (3)
0 Kudos
Reply
1 Solution
2,877 Views
jay_heng
NXP Employee
NXP Employee

eFUSE 0x840[3] bit should be burnt to enable XECC module, or XECC is inactive by default.

See my blog for XECC enablement.

https://www.cnblogs.com/henjay724/p/15204125.html

View solution in original post

0 Kudos
Reply
2 Replies
2,874 Views
Ootsuka
Contributor II

Thank you very much for answer.

0 Kudos
Reply
2,878 Views
jay_heng
NXP Employee
NXP Employee

eFUSE 0x840[3] bit should be burnt to enable XECC module, or XECC is inactive by default.

See my blog for XECC enablement.

https://www.cnblogs.com/henjay724/p/15204125.html

0 Kudos
Reply