SD_HostInit Fails

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SD_HostInit Fails

1,731 次查看
omerkaanbasakin
Contributor IV

Hi ı am using imrt1052 on custom board and ı am using mcuxpresso , SDK_2.7.0_MIMXRT1052xxxxB. 

I modified sdcard_fatfs_freertos example and it worked. But when ı create a new project, host init fails. 

My modifications on example:

removed vselect pin, sd card use 3.3v.

changed sd_cd_sw pin  to GPIO2 24

change code in board.h to

 #define BOARD_USDHC_CD_GPIO_BASE GPIO2
#define BOARD_USDHC_CD_GPIO_PIN 24
#define BOARD_USDHC_CD_PORT_IRQ GPIO2_Combined_16_31_IRQn
#define BOARD_USDHC_CD_PORT_IRQ_HANDLER GPIO2_Combined_16_31_IRQHandler

and because of the custom board design

sd_cd_sw signal work reverse so ı changed 

#define BOARD_HAS_SDCARD (1U)

#define BOARD_USDHC_CARD_INSERT_CD_LEVEL (0U)

to 

#define BOARD_HAS_SDCARD (0U)

#define BOARD_USDHC_CARD_INSERT_CD_LEVEL (1U)

code works well like this

created project:

copied the code below into the board.h 

#define BOARD_USDHC1_BASEADDR USDHC1
#define BOARD_USDHC2_BASEADDR USDHC2
#define BOARD_USDHC_CD_GPIO_BASE GPIO2
#define BOARD_USDHC_CD_GPIO_PIN 24
#define BOARD_USDHC_CD_PORT_IRQ GPIO2_Combined_16_31_IRQn
#define BOARD_USDHC_CD_PORT_IRQ_HANDLER GPIO2_Combined_16_31_IRQHandler

#define BOARD_USDHC_CD_STATUS() (GPIO_PinRead(BOARD_USDHC_CD_GPIO_BASE, BOARD_USDHC_CD_GPIO_PIN))

#define BOARD_USDHC_CD_INTERRUPT_STATUS() (GPIO_PortGetInterruptFlags(BOARD_USDHC_CD_GPIO_BASE))
#define BOARD_USDHC_CD_CLEAR_INTERRUPT(flag) (GPIO_PortClearInterruptFlags(BOARD_USDHC_CD_GPIO_BASE, flag))

#define BOARD_USDHC_CD_GPIO_INIT() \
{ \
gpio_pin_config_t sw_config = { \
kGPIO_DigitalInput, \
0, \
kGPIO_IntRisingOrFallingEdge, \
}; \
GPIO_PinInit(BOARD_USDHC_CD_GPIO_BASE, BOARD_USDHC_CD_GPIO_PIN, &sw_config); \
GPIO_PortEnableInterrupts(BOARD_USDHC_CD_GPIO_BASE, 1U << BOARD_USDHC_CD_GPIO_PIN); \
GPIO_PortClearInterruptFlags(BOARD_USDHC_CD_GPIO_BASE, ~0); \
}
#define BOARD_HAS_SDCARD (0U)
#define BOARD_SD_POWER_RESET_GPIO (GPIO1)
#define BOARD_SD_POWER_RESET_GPIO_PIN (5U)

#define BOARD_USDHC_CARD_INSERT_CD_LEVEL (1U)

#define BOARD_USDHC_MMCCARD_POWER_CONTROL(state)

#define BOARD_USDHC_MMCCARD_POWER_CONTROL_INIT() \
{ \
gpio_pin_config_t sw_config = { \
kGPIO_DigitalOutput, \
0, \
kGPIO_NoIntmode, \
}; \
GPIO_PinInit(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, &sw_config); \
GPIO_PinWrite(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, true); \
}

#define BOARD_USDHC_SDCARD_POWER_CONTROL_INIT() \
{ \
gpio_pin_config_t sw_config = { \
kGPIO_DigitalOutput, \
0, \
kGPIO_NoIntmode, \
}; \
GPIO_PinInit(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, &sw_config); \
}

#define BOARD_USDHC_SDCARD_POWER_CONTROL(state) \
(GPIO_PinWrite(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, state))

#define BOARD_USDHC1_CLK_FREQ (CLOCK_GetSysPfdFreq(kCLOCK_Pfd0) / (CLOCK_GetDiv(kCLOCK_Usdhc1Div) + 1U))
#define BOARD_USDHC2_CLK_FREQ (CLOCK_GetSysPfdFreq(kCLOCK_Pfd0) / (CLOCK_GetDiv(kCLOCK_Usdhc2Div) + 1U))

#define BOARD_SD_HOST_BASEADDR BOARD_USDHC1_BASEADDR
#define BOARD_SD_HOST_CLK_FREQ BOARD_USDHC1_CLK_FREQ
#define BOARD_SD_HOST_IRQ USDHC1_IRQn

#define BOARD_MMC_HOST_BASEADDR BOARD_USDHC2_BASEADDR
#define BOARD_MMC_HOST_CLK_FREQ BOARD_USDHC2_CLK_FREQ
#define BOARD_MMC_HOST_IRQ USDHC2_IRQn
#define BOARD_MMC_VCCQ_SUPPLY kMMC_VoltageWindow170to195
#define BOARD_MMC_VCC_SUPPLY kMMC_VoltageWindows270to360
/* we are using the BB SD socket to DEMO the MMC example,but the
* SD socket provide 4bit bus only, so we define this macro to avoid
* 8bit data bus test
*/
#define BOARD_MMC_SUPPORT_8BIT_BUS (1U)

#define BOARD_SD_HOST_SUPPORT_SDR104_FREQ (200000000U)
#define BOARD_SD_HOST_SUPPORT_HS200_FREQ (180000000U)

and copied examples board.c to my projects board.c folder.

Copied source folder to my projects source folder. 

ıt not worked.Sd_HostInit fails. Cant find the solution. 

p.s. attached my project 

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

1,650 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Could you please provide more information about the problem that you are facing? For example, in the new project that you created when you call the function Sd_HostInit, what is happening? Does your application crash? If so, where exactly does it crash? Does it return an error? If so, which error? 

Regards, 

Victor 

0 项奖励
回复

1,650 次查看
omerkaanbasakin
Contributor IV

Hi victorjimenez

Thanks for your reply, 

Yes project prints SD_HostInit Fail to console. Debug session stops. Not sure what is the problem but I created another project , change code above and change usb Clock 198Mhz, ARM clock 600MHz . Project sucessfully works.

Kind Regards.

0 项奖励
回复