Rt600 clock configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Rt600 clock configuration

1,120 次查看
Tay
Contributor I

Hello,

I'm using the MIMXRT685, I want the system clock ti be 160Mhz. I tried to change the clock configuration using MCUXpresso config tools but apparently it doesn't support this device. Can u help?

Thank u

0 项奖励
回复
1 回复

1,094 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hello Tay,

Please try to use latest version of IDE and SDK. I used MCUXpresso IDE v11.2.1 and SDK 2.8.2 to test this and I was able to set system clock to 160 MHz using MCUXpresso Config Tools. Please check the image below.

image.png

Hope it helps!

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 项奖励
回复