Rt1052 Compiling and running with arm-none-eabi-gcc does not work in sdrma

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Rt1052 Compiling and running with arm-none-eabi-gcc does not work in sdrma

跳至解决方案
1,968 次查看
wandongli
Contributor I

      I migrated the project under keil to linux and compiled it with gcc. The MIMXRT1052xxxxx_flexspi_nor.ld script in sdk2.3 works fine, but it does not work with MIMXRT1052xxxxx_sdram_txt.ld.I uploaded my project, please help me to see it, after the normal download, the serial port will have output, the baud rate is 921600.

标签 (1)
0 项奖励
回复
1 解答
1,875 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi wangdong,

   Do you try the RT1050 newest SDK code sdk2.5.0?

   Which can be downloaded from this link:

  Welcome | MCUXpresso SDK Builder 

   Whether the official code works OK on your side or not?

 


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,876 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi wangdong,

   Do you try the RT1050 newest SDK code sdk2.5.0?

   Which can be downloaded from this link:

  Welcome | MCUXpresso SDK Builder 

   Whether the official code works OK on your side or not?

 


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复