Hi
Could you please recommend a RT device that supports 2-channel camera input and display at same time?
The application is similart with 2ch-dash cam.
Regards,
Jack
Hi @JK-IMX ,
May I consider you want to use two CSI at the same time?
If yes, we recommend you one use the CSI API, another use the flexIO to simulate the CSI to connect your camera.
Normal CSI, you can refer to the RT SDK CSI code, flexIO emulate CSI, please refer to this AN:
https://www.nxp.com/docs/en/application-note/AN12686.pdf
https://www.nxp.com/docs/en/application-note-software/AN12686SW.zip
Wish it helps you!
Best Regards,
Kerry