Hi all,
I am currently working with the NXP i.MX RT1176 controller and looking to implement IP camera streaming functionality directly from the controller. For this, I need to integrate RTSP (Real-Time Streaming Protocol) to enable video streaming over Ethernet.
As of now, I haven’t found any example projects or reference implementations of RTSP streaming on the RT1176 platform. I would appreciate any guidance, examples, or recommendations on:
RTSP client or server implementation on RT1176
Streaming video using RTSP over Ethernet or Wi-Fi
Whether anyone has successfully used LIVE555 or similar lightweight RTSP stacks with the RT1176
If NXP or the community has any reference designs or SDKs that include RTSP streaming (e.g., related to SLN-TLHMI-IOT-RD or SLN-VIZNAS-IOT), that would also be very helpful.
Thanks in advance!