Hello,
I'm running SAI3 in BCLK/SYNC slave mode and experience glitches which lead to sync errors, i.e. SEF interrupt (section 58.3.6.4). There seems to be no internal glitch filter on these clock inputs.
My question is: Does the RT1176 support input hysteresis?
Figure 13-3 and section 13.3.1.1.1 in the reference manual describe such a feature but I cannot find a way to enable that in the SW_PAD_CTL_xxx registers.
Thanks.
Udo
解決済! 解決策の投稿を見る。
Hello, sorry for the late response, I was researching more information.
All IO support the hysteresis. and for datasheet, it only provide the input hysteresis value for GPIO_AD/GPIO_LPSR/GPIO_DISP_B2, and for GPIO_EMC_B2, it take the different IO lib, and the design don't provide the input hysteresis value in current datasheet, but it still support input hysteresis.
Best regards,
Pavel
Hi Pavel,
Thanks for your reply. I wasn't using RM Rev 2 for some reason, still had Rev 1.
This question remains: Which pins do actually support input hysteresis?
In the datasheet (IMXRT1170CEC, Rev. 4, 05/2023) I found an "Input Hysteresis" parameter in Table 37 which applies to GPIO_AD/GPIO_LPSR/GPIO_DISP_B2. However, I'm using GPIO_EMC_B2. This would be Table 35 which does not list such a parameter. So can I assume that GPIO_EMC_B2 pins do not implement hysteresis?
Best regards,
Udo
Hello, sorry for the late response, I was researching more information.
All IO support the hysteresis. and for datasheet, it only provide the input hysteresis value for GPIO_AD/GPIO_LPSR/GPIO_DISP_B2, and for GPIO_EMC_B2, it take the different IO lib, and the design don't provide the input hysteresis value in current datasheet, but it still support input hysteresis.
Best regards,
Pavel
Thank you for the information. This is very helpful.
Best regards,
Udo
Hello, I saw this note on the RM.
Document Number: IMXRT1170RM
Rev. 2, 06/2023
Best regards,
Pavel
Hello, my name is Pavel, and I will be supporting your case, let me get into your case and when I have more information, I will contact you.
Best regards,
Pavel