RT1176 EVK running failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1176 EVK running failed

887 次查看
macro_lee
Contributor I

mdk keil (RT1176 EVK):

when i select the flexspi_nor_sdram release project,after i rebuild it and load to the rt1176,evk board can not run well (just like dead crash),the same with putting the reset button;

when i select the flexspi_nor_sdram debug project,after i rebuild it and load to the rt1176,evk board can run well(debug run and then stoped the debug window),but when i putting the reset button;the evk board crashed;

i try to using the secure provising tool to connect the evk board but always failed(through the sdp usb port, tip: boot mode (both 00 and 01 all used to try))

that‘s why, thanks for your help

Best Regards!

0 项奖励
回复
1 回复

830 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If you are doing all ok the is probably that you have a damage board, please contact your vendor for this reason.

Regards

0 项奖励
回复