RT1172 using a 3-wire spi mode to configure lvds panel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1172 using a 3-wire spi mode to configure lvds panel

1,206 次查看
shawn_123
Contributor I

hello dear nxp engineer

    I am using a rt1172 MCU want to connect a lvds panel, this panel is from a small company, which is configure via 3-wire spi the image format is 18bit RGB. 

my first question is from the SDK example i found the lpspi example incude polling/b2b/interrupt  i am not so familiar with this mcu, how to configure the 3-wire spi, so i can write cmd and  data the configure the panel in the initialization process. i learned that 3-wire spi only using CS, SCLK,and a bi-directional IO wire. how to change the lpspi demo to code to achieve this target, or i need to rewrite it totally, please give some help or doc support, thanks a lot!

 

0 项奖励
回复
1 回复

1,156 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @shawn_123,

Please look into the following community post about 3-wire SPI on RT1170: https://community.nxp.com/t5/i-MX-RT/3-wire-SPI-on-RT1170/td-p/1643360

I believe it will prove very useful for your inquiry. If you have further questions about this topic, don't hesitate on letting me know.

BR,
Edwin.

0 项奖励
回复