RT1170 usb dev hid detection problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1170 usb dev hid detection problem

164 Views
dskim2
Contributor III

Hi

I tested evkbmimxrt1170_dev_hid_generic_bm_cm7 example with MiMXRT1170-EVKB.

It is work well.

I want to use flexspi nor flash and dev hid usb in the same project.

I added the linkscript from evkbmimxrt1170_flexspi_nor_polling_transfer_cm7 to evkbmimxrt1170_dev_hid_generic_bm_cm7.

dskim2_3-1725861428797.png

 

But the EVK was not detected.

dskim2_1-1725861365712.png

If linkscript is not added to the project, the USB is recognized, but flash related functions do not work.

How can I solve this?

Please see attatched source zip file.

Best Regards

 

0 Kudos
Reply
1 Reply

140 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @dskim2,

Due to the complexity and dependencies of the FlexSPI example code, I would recommend you port the USB capabilities to the FlexSPI example, rather than the FlexSPI capabilities to the USB example. On the evkbmimxrt1170_flexspi_nor_polling_transfer_cm7, add the USB component using the "Manage SDK components" window, and then copy and paste the code from evkbmimxrt1170_dev_hid_generic_bm_cm7 that you wish to incorporate into the project.

BR,
Edwin.

0 Kudos
Reply