RT1160 Dual Image support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1160 Dual Image support

Jump to solution
487 Views
iann
Contributor III

Hi for the application we're developing using the MIMXRT1166 we're looking at whether the internal boot ROM is enough to handle our program updates in the field. The Dual image support sounds very useful but there isn't much information apart from 10.13.3 Enter Bootloader API in the Reference Manual

Enter bootloader.png

but it isn't mentioned again.

Are there further app notes or SDK examples where this is elaborated on?

I found some more information in the IMXRT1170RM 

Dual image IMXRT1170.png

Does this also apply to the RT1160 parts?

Thanks for any help

Ian Norman

0 Kudos
Reply
1 Solution
445 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @iann 

Yes, dual image support should also apply for RT1160.

Currently, we have this document Pi Ziheng Embedded: Revealing the alternate boot design of serial NOR Flash dual programs on i.MXRT1... . This article was written  by a chinese colleague, in chinese, please translate it to english. 

I hope this could help you. 

Diego

View solution in original post

0 Kudos
Reply
2 Replies
446 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @iann 

Yes, dual image support should also apply for RT1160.

Currently, we have this document Pi Ziheng Embedded: Revealing the alternate boot design of serial NOR Flash dual programs on i.MXRT1... . This article was written  by a chinese colleague, in chinese, please translate it to english. 

I hope this could help you. 

Diego

0 Kudos
Reply
434 Views
iann
Contributor III
Thank you very much for confirming, and the extra document is very helpful.

Ian