RT1170 series microcontroller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1170 series microcontroller

3,565 次查看
AyushiAgrawal
Contributor I

 RT1170 series MIMXRT1176DVMAA microcontroller supports upto 2 EMV SIM modules.

May I get the more details of these SIM modules whether support 4G/5G/ LTE or not?

When buying this NXP controller then what are the connectors and Module part number that I also require along with it?

In short, I want to have the GSM/GPRS - 4g/5g/ LTE with this RT series microcontroller so can I achieve that?

0 项奖励
回复
6 回复数

3,487 次查看
robSanders
NXP Employee
NXP Employee

I think the question is - does the EMV SIM module require an external IC to interface with an eSIM? This mobile POS reference design seems to indicate so (TDA8034), although I don't think the data sheet necessarily clarifies this. @jingpan any thoughts on this? 

0 项奖励
回复

3,446 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

The EMVSIM on RT1170 compatible with ISO7816-3 and EMV v4.3. It can connect to sim card directly. But the TDA8034 can give more, such as level shift, protection and enhanced ESD. Using an external IC like TDA8034 is good for the design.

 

Regards,

Jing

0 项奖励
回复

3,546 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi AyushiAgrawal,

Yes, RT1170 EMVSIM port can support GSM/4G/5G sim card. Their hardware interface is same.

 

Regards,

Jing

0 项奖励
回复

3,531 次查看
AyushiAgrawal
Contributor I

May I get the more details over it since we are planning to use this NXP microcontroller?

Does controller has EMV slots in microcontroller ,( I am not talking of evaluation board) and what are the other requirements to make it work as a GSM 4G 5G?

0 项奖励
回复

3,524 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Sorry, but what do you mean of "Does controller has EMV slots in microcontroller"? RT1170 reference manual and datasheet is released. Please refer to it.

 

Regards,

Jing

0 项奖励
回复

3,521 次查看
AyushiAgrawal
Contributor I

 Hi,

Sorry to bother you but yes I looked the reference manual and the datasheet but it does not bring much clarity on the requirements to make it work for 4G/ 5G LTE. 

AyushiAgrawal_0-1611901422807.png

 

0 项奖励
回复