RT1170: error in documentation or in config tool?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1170: error in documentation or in config tool?

441 次查看
mastupristi
Senior Contributor I

Hello,

in the SAI chapter of the Ref Man rev3, you can find this table:

SAI_MCLK_table.png

There are some perplexing points:

  1. It seems that SAI1 cannot be fed by MCLK pin as other SAIs, and it has sai*_ipg_clk_sai_mclk selectable
  2. SAI3 seems to be able to be powered only by sai2_clk_root, instead of sai3_clk_root.
  3. SAI4 seems to have enabled only one option (MCLK pin) and no sai4_clk_root option at all.

but on MCUXpresso Config Tools 24.12 I see:

SAI_config_tool15.png

 

Looking at this diagram I can rewrite the points above:

  1. sai*_ipg_clk_sai_mclk seems to be the same of SAI*_MCLK pin
  2. SAI3 seems to be able to be powered by SAI3_CLK_ROOT
  3. SAI4 seems to have 2 option enabled including SAI4_CLK_ROOT as well as SAI4_MCLK pin

I believe that the documentation has “problems” and needs revision. Anyway please share with me, because maybe it could be Config Tool that is buggy.

 

best regards

Max

0 项奖励
回复
1 回复

397 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Thank you for your feedback, indeed the confusion is on the documentation side. Your 3 points are correct. From my side let me give these comments to the team responsible for the communication.

Best regards,
Omar

0 项奖励
回复