RT1170 SEMC_AD11/12 state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1170 SEMC_AD11/12 state

ソリューションへジャンプ
766件の閲覧回数
Eugene3
Contributor II

Hi

I'm using RT1170 for my board. I connect SDRAM and SRAM on the SEMC bus.

Is it possible to set SEMC_ADDRESS11 & 12 to High or HighZ while SEMC doesn't access SDRAM or SRAM?

 

SEMC_ADDRESS11 & 12 are WE# and OE# for SRAM, so I'd like to set these pins to inactive state while SEMC is not accessing SRAM.

0 件の賞賛
返信
1 解決策
730件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Eugene3,

The only moment where a pin is High-Z is after a reset. Once initialized, the pin will no longer be High-Z unless doing a full POR once again. For this reason, the SEMC_ADDRESS11 and 12 cannot be set to High-Z. You can definitely deinitialize these pins when not in use, but this will not set them to high impedance.

BR,
Edwin.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
731件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Eugene3,

The only moment where a pin is High-Z is after a reset. Once initialized, the pin will no longer be High-Z unless doing a full POR once again. For this reason, the SEMC_ADDRESS11 and 12 cannot be set to High-Z. You can definitely deinitialize these pins when not in use, but this will not set them to high impedance.

BR,
Edwin.

0 件の賞賛
返信