RT116x/7x Inline Encryption Engine performance with SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT116x/7x Inline Encryption Engine performance with SDRAM

1,349 次查看
stephenschwartz
Contributor II

Hello,

I have read in the Security Reference Manual for the i.MXRT1170 how the IEE peripheral can be used to decrypt data from SDRAM without software intervention. Is it possible to use the IEE to decrypt code that is executing from SDRAM? If so, is there any latency added by using the IEE?

Thanks,

Steve Schwartz-Fenwick

0 项奖励
回复
1 回复

1,330 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

IEE can be used when you have an encrypted XIP(execute in place) image booting from FlexSPI.
In SDRAM the IEE module can be used to encrypt/decrypt data.

If you have more questions do not hesitate to ask me.
Best regards,
Omar
 

0 项奖励
回复