RT116x/7x Inline Encryption Engine performance with SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT116x/7x Inline Encryption Engine performance with SDRAM

1,343件の閲覧回数
stephenschwartz
Contributor II

Hello,

I have read in the Security Reference Manual for the i.MXRT1170 how the IEE peripheral can be used to decrypt data from SDRAM without software intervention. Is it possible to use the IEE to decrypt code that is executing from SDRAM? If so, is there any latency added by using the IEE?

Thanks,

Steve Schwartz-Fenwick

0 件の賞賛
返信
1 返信

1,324件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

IEE can be used when you have an encrypted XIP(execute in place) image booting from FlexSPI.
In SDRAM the IEE module can be used to encrypt/decrypt data.

If you have more questions do not hesitate to ask me.
Best regards,
Omar
 

0 件の賞賛
返信