RT116x/7x Inline Encryption Engine performance with SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT116x/7x Inline Encryption Engine performance with SDRAM

1,348 Views
stephenschwartz
Contributor II

Hello,

I have read in the Security Reference Manual for the i.MXRT1170 how the IEE peripheral can be used to decrypt data from SDRAM without software intervention. Is it possible to use the IEE to decrypt code that is executing from SDRAM? If so, is there any latency added by using the IEE?

Thanks,

Steve Schwartz-Fenwick

0 Kudos
Reply
1 Reply

1,329 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

IEE can be used when you have an encrypted XIP(execute in place) image booting from FlexSPI.
In SDRAM the IEE module can be used to encrypt/decrypt data.

If you have more questions do not hesitate to ask me.
Best regards,
Omar
 

0 Kudos
Reply