RT106x external interrupt sources

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT106x external interrupt sources

1,991件の閲覧回数
mszczygi
Contributor I

Hi,

Is there a document that describe assignment of external interrupt sources to interrupt controller in i.MX RT1060/1064?

What I'm asking is, for example, I have a external trigger source, like push button, connected to GPIO pin that should trigger interrupt handler function. I'm designing hardware base on i.MX RT1060 and I'd like to know which GPIO's pins can be used as source for external interrupt. In my experience with ARM Cortex-M micro-controllers only certain number of GPIOs can be assign to function as trigger sources for external interrupts.

Best regards

Mariusz

ラベル(5)
0 件の賞賛
返信
1 返信

1,886件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Mariusz,

Regarding your following question: "I'd like to know which GPIO's pins can be used as a source for external interrupt". You can find this information on Table 3-2 of the reference manual.

pastedImage_1.png

Also, within the SDK for the RT1060-EVK you will find an example named igpio_input_interrupt. This project triggers an interrupt each time you press a button from the evaluation kit. You can use this project as a base to create your own. 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信