[RT106F] Is ML Vision Engine optimized for RT106F in NXP OASIS LITE runtime library?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[RT106F] Is ML Vision Engine optimized for RT106F in NXP OASIS LITE runtime library?

1,256 次查看
dave_choi
Contributor II

Hello, everyone.

Is ML Vision Engine optimized for RT106F in NXP OASIS LITE Tuntime library?

If RT106F runs at 600Hz, if a better performance MCU is used, can the ML Vision Engine performance be improved? Or is it already optimized for RT106F?

Thank you for your attention.

0 项奖励
回复
1 回复

1,241 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is ML Vision Engine optimized for RT106F in NXP OASIS LITE Tuntime library?
-- Yes.
2) If RT106F runs at 600 Hz, if a better performance MCU is used, can the ML Vision Engine performance be improved? Or is it already optimized for RT106F?
-- The inference speed of ML Vision Engine performance will be improved when RT106F runs at a higher frequency clock.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复