RT1064 LPI2C Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1064 LPI2C Problem

3,344 Views
lixuhui112
Contributor I

in RT1064 I wan to use LPI2C ,

i use MCUXpreso IDE and SDK use SDK_2_10_0_MIMXRT1064xxxxA

use demo evkmimxrt1064_lpi2c_polling_b2b_master

but find a problem:

LPI2C only send start singe

LPI2C send singeLPI2C send singe

pin config 

 

 

pin configpin config

 

code :

/*
* Copyright 2017 NXP
* All rights reserved.
*
* SPDX-License-Identifier: BSD-3-Clause
*/

/* Standard C Included Files */
#include <stdio.h>
#include <string.h>
#include "pin_mux.h"
#include "clock_config.h"
#include "board.h"
#include "fsl_debug_console.h"
#include "fsl_lpi2c.h"

/*******************************************************************************
* Definitions
******************************************************************************/
#define EXAMPLE_I2C_MASTER_BASE (LPI2C3_BASE)

/* Select USB1 PLL (480 MHz) as master lpi2c clock source */
#define LPI2C_CLOCK_SOURCE_SELECT (0U)
/* Clock divider for master lpi2c clock source */
#define LPI2C_CLOCK_SOURCE_DIVIDER (5U)
/* Get frequency of lpi2c clock */
#define LPI2C_CLOCK_FREQUENCY ((CLOCK_GetFreq(kCLOCK_Usb1PllClk) / / (LPI2C_CLOCK_SOURCE_DIVIDER + 1U))

#define LPI2C_MASTER_CLOCK_FREQUENCY LPI2C_CLOCK_FREQUENCY
#define WAIT_TIME 10U


#define EXAMPLE_I2C_MASTER ((LPI2C_Type *)EXAMPLE_I2C_MASTER_BASE)

#define LPI2C_MASTER_SLAVE_ADDR_7BIT 0x7EU
#define LPI2C_BAUDRATE 100000U
#define LPI2C_DATA_LENGTH 33U

/*******************************************************************************
* Prototypes
******************************************************************************/

/*******************************************************************************
* Variables
******************************************************************************/

uint8_t g_master_txBuff[LPI2C_DATA_LENGTH];
uint8_t g_master_rxBuff[LPI2C_DATA_LENGTH];

/*******************************************************************************
* Code
******************************************************************************/

/*!
* @brief Main function
*/
int lpi2c_test(void)
{
lpi2c_master_config_t masterConfig;
status_t reVal = kStatus_Fail;
uint8_t deviceAddress = 0x01U;
size_t txCount = 0xFFU;

 

/*Clock setting for LPI2C*/
CLOCK_SetMux(kCLOCK_Lpi2cMux, LPI2C_CLOCK_SOURCE_SELECT);
CLOCK_SetDiv(kCLOCK_Lpi2cDiv, LPI2C_CLOCK_SOURCE_DIVIDER);

PRINTF("\r\nLPI2C board2board polling example -- Master transfer.\r\n");

/* Set up i2c master to send data to slave*/
/* First data in txBuff is data length of the transmiting data. */
g_master_txBuff[0] = LPI2C_DATA_LENGTH - 1U;
for (uint32_t i = 1U; i < LPI2C_DATA_LENGTH; i++)
{
g_master_txBuff[i] = i - 1;
}

PRINTF("Master will send data :");
for (uint32_t i = 0U; i < LPI2C_DATA_LENGTH - 1U; i++)
{
if (i % 8 == 0)
{
PRINTF("\r\n");
}
PRINTF("0x%2x ", g_master_txBuff[i + 1]);
}
PRINTF("\r\n\r\n");

/*
* masterConfig.debugEnable = false;
* masterConfig.ignoreAck = false;
* masterConfig.pinConfig = kLPI2C_2PinOpenDrain;
* masterConfig.baudRate_Hz = 100000U;
* masterConfig.busIdleTimeout_ns = 0;
* masterConfig.pinLowTimeout_ns = 0;
* masterConfig.sdaGlitchFilterWidth_ns = 0;
* masterConfig.sclGlitchFilterWidth_ns = 0;
*/
LPI2C_MasterGetDefaultConfig(&masterConfig);

/* Change the default baudrate configuration */
masterConfig.baudRate_Hz = LPI2C_BAUDRATE;

/* Initialize the LPI2C master peripheral */
LPI2C_MasterInit(EXAMPLE_I2C_MASTER, &masterConfig, LPI2C_MASTER_CLOCK_FREQUENCY);

/* Send master blocking data to slave */
if (kStatus_Success == LPI2C_MasterStart(EXAMPLE_I2C_MASTER, LPI2C_MASTER_SLAVE_ADDR_7BIT, kLPI2C_Write))
{
/* Check master tx FIFO empty or not */
LPI2C_MasterGetFifoCounts(EXAMPLE_I2C_MASTER, NULL, &txCount);
while (txCount)
{
LPI2C_MasterGetFifoCounts(EXAMPLE_I2C_MASTER, NULL, &txCount);
}
/* Check communicate with slave successful or not */
if (LPI2C_MasterGetStatusFlags(EXAMPLE_I2C_MASTER) & kLPI2C_MasterNackDetectFlag)
{
return kStatus_LPI2C_Nak;
}

/* subAddress = 0x01, data = g_master_txBuff - write to slave.
start + slaveaddress(w) + subAddress + length of data buffer + data buffer + stop*/
reVal = LPI2C_MasterSend(EXAMPLE_I2C_MASTER, &deviceAddress, 1);
if (reVal != kStatus_Success)
{
if (reVal == kStatus_LPI2C_Nak)
{
LPI2C_MasterStop(EXAMPLE_I2C_MASTER);
}
return -1;
}

reVal = LPI2C_MasterSend(EXAMPLE_I2C_MASTER, g_master_txBuff, LPI2C_DATA_LENGTH);
if (reVal != kStatus_Success)
{
if (reVal == kStatus_LPI2C_Nak)
{
LPI2C_MasterStop(EXAMPLE_I2C_MASTER);
}
return -1;
}

reVal = LPI2C_MasterStop(EXAMPLE_I2C_MASTER);
if (reVal != kStatus_Success)
{
return -1;
}
}

/* Wait until the slave is ready for transmit, wait time depend on user's case.
Slave devices that need some time to process received byte or are not ready yet to
send the next byte, can pull the clock low to signal to the master that it should wait.*/
for (uint32_t i = 0U; i < WAIT_TIME; i++)
{
__NOP();
}

PRINTF("Receive sent data from slave :");

/* Receive blocking data from slave */
/* subAddress = 0x01, data = g_master_rxBuff - read from slave.
start + slaveaddress(w) + subAddress + repeated start + slaveaddress(r) + rx data buffer + stop */
if (kStatus_Success == LPI2C_MasterStart(EXAMPLE_I2C_MASTER, LPI2C_MASTER_SLAVE_ADDR_7BIT, kLPI2C_Write))
{
/* Check master tx FIFO empty or not */
LPI2C_MasterGetFifoCounts(EXAMPLE_I2C_MASTER, NULL, &txCount);
while (txCount)
{
LPI2C_MasterGetFifoCounts(EXAMPLE_I2C_MASTER, NULL, &txCount);
}
/* Check communicate with slave successful or not */
if (LPI2C_MasterGetStatusFlags(EXAMPLE_I2C_MASTER) & kLPI2C_MasterNackDetectFlag)
{
return kStatus_LPI2C_Nak;
}

reVal = LPI2C_MasterSend(EXAMPLE_I2C_MASTER, &deviceAddress, 1);
if (reVal != kStatus_Success)
{
if (reVal == kStatus_LPI2C_Nak)
{
LPI2C_MasterStop(EXAMPLE_I2C_MASTER);
}
return -1;
}

reVal = LPI2C_MasterRepeatedStart(EXAMPLE_I2C_MASTER, LPI2C_MASTER_SLAVE_ADDR_7BIT, kLPI2C_Read);
if (reVal != kStatus_Success)
{
return -1;
}

reVal = LPI2C_MasterReceive(EXAMPLE_I2C_MASTER, g_master_rxBuff, LPI2C_DATA_LENGTH - 1);
if (reVal != kStatus_Success)
{
if (reVal == kStatus_LPI2C_Nak)
{
LPI2C_MasterStop(EXAMPLE_I2C_MASTER);
}
return -1;
}

reVal = LPI2C_MasterStop(EXAMPLE_I2C_MASTER);
if (reVal != kStatus_Success)
{
return -1;
}
}

for (uint32_t i = 0U; i < LPI2C_DATA_LENGTH - 1; i++)
{
if (i % 8 == 0)
{
PRINTF("\r\n");
}
PRINTF("0x%2x ", g_master_rxBuff[i]);
}
PRINTF("\r\n\r\n");

/* Transfer completed. Check the data.*/
for (uint32_t i = 0U; i < LPI2C_DATA_LENGTH - 1U; i++)
{
if (g_master_rxBuff[i] != g_master_txBuff[i + 1])
{
PRINTF("\r\nError occurred in the transfer ! \r\n");
break;
}
}

PRINTF("\r\nEnd of LPI2C example .\r\n");
while (1)
{
}
}

 

Labels (1)
0 Kudos
Reply
2 Replies

3,315 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.
I was able to replicate running the example with SDK version(2.10.0) and the results were successful.

Omar_Anguiano_0-1636428091835.png

I suggest you check if this issue persists with LPI2C1 and the default pin configuration from the example.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply

3,342 Views
lixuhui112
Contributor I

but I use the same demo in MIMXRT1060-EVK it is ok

0 Kudos
Reply