RT1060 - SDRAM Initialization Script

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1060 - SDRAM Initialization Script

ソリューションへジャンプ
3,521件の閲覧回数
pauricacre
Contributor III

Is there an initialization script for debugging SDRAM in MCUXpresso using CMSIS-DAP on the RT1060? I cant find one. I'm unable to debug my EVK when my application is set to run in SDRAM.

 

0 件の賞賛
返信
1 解決策
3,500件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

You can download the script from the following link: 

Overview of using the MIMXRT1050-EVK(B) with MCUXp... - NXP Community

Although the script says that it's for the RT1050-EVKB, the RT1060-EVK has the same SDRAM. The pdf document explains how to use this script. 

Regards,
Victor 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,501件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

You can download the script from the following link: 

Overview of using the MIMXRT1050-EVK(B) with MCUXp... - NXP Community

Although the script says that it's for the RT1050-EVKB, the RT1060-EVK has the same SDRAM. The pdf document explains how to use this script. 

Regards,
Victor 

0 件の賞賛
返信