Hi,
Thanks for your reply.
1) So every time I need to use Config Tool of Clock to calculate the clock rate then update the code to get the target clock, right?
-- In general, it's right.
2) CLOCK_GetFreq() function is able to provide the required clock's frequency, but there's no function to indicate the CPU usage in the SDK library until now.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------