RT105X IAR flashloader source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT105X IAR flashloader source code

1,880 Views
echozeng
Contributor III

I want to modify and rebuild rt105x IAR flashloader(..\arm\config\flashloader\NXP\FlashIMXRT1050_EVK_FlexSPI.out).

Where can I get IAR flashloader source code?

Thanks.

0 Kudos
Reply
1 Reply

1,719 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi echo zeng

Unfortunately, IAR systems provide this .out to be used as it is, so you cannot modify these files and the source code is not given by IAR system. However, you can check the document:

http://supp.iar.com/FilesPublic/UPDINFO/004916/arm/doc/FlashLoaderGuide.pdf 

Page 8, it mentioned that process to create a custom flashloader with IAR.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply