RT105X IAR flashloader source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT105X IAR flashloader source code

1,923件の閲覧回数
echozeng
Contributor III

I want to modify and rebuild rt105x IAR flashloader(..\arm\config\flashloader\NXP\FlashIMXRT1050_EVK_FlexSPI.out).

Where can I get IAR flashloader source code?

Thanks.

0 件の賞賛
返信
1 返信

1,762件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi echo zeng

Unfortunately, IAR systems provide this .out to be used as it is, so you cannot modify these files and the source code is not given by IAR system. However, you can check the document:

http://supp.iar.com/FilesPublic/UPDINFO/004916/arm/doc/FlashLoaderGuide.pdf 

Page 8, it mentioned that process to create a custom flashloader with IAR.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信