RT1020 Bus Encryption Engine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1020 Bus Encryption Engine

2,743 Views
rshipman
Senior Contributor I

Hi,

Does the Bus Encryption Engine encrypt as well as decrypt?

For example, if I was running an Encrypted XIP application (from serial nor flash), and I wanted it to write something to a different area of flash, what happens? Is it encrypted when writing, and decrypted when reading? Or are all read/writes to flash in plaintext, and only reads of the bootable image decrypted on the fly?

Many thanks.

Labels (2)
0 Kudos
Reply
2 Replies

2,657 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Does the Bus Encryption Engine encrypt as well as decrypt?

No, the BEE is implemented as an on-the-fly decryption engine only. 


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,210 Views
BYD_LV
Contributor I
What should I do if I have access to flash and write data to flash at the same time?
0 Kudos
Reply