RT1015 Write multiple GPIO at same time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1015 Write multiple GPIO at same time

1,443 次查看
kensu
Contributor V

Hi,

Can RT1015 write multiple GPIO at same time?

Regards

Ken

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,386 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ken Su

  If you check the GPIO register, it is not difficult to find, you can operate upto 32 GPIOs at the same time.

pastedImage_1.png

Because you can find the DR register can write each bit at the same time.

With it helps you!

     If you still have question about it, please kindly let me know.

 

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复