RT1015 Write multiple GPIO at same time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1015 Write multiple GPIO at same time

1,457件の閲覧回数
kensu
Contributor V

Hi,

Can RT1015 write multiple GPIO at same time?

Regards

Ken

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,400件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ken Su

  If you check the GPIO register, it is not difficult to find, you can operate upto 32 GPIOs at the same time.

pastedImage_1.png

Because you can find the DR register can write each bit at the same time.

With it helps you!

     If you still have question about it, please kindly let me know.

 

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信