RT1015 Write multiple GPIO at same time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1015 Write multiple GPIO at same time

1,441 Views
kensu
Contributor V

Hi,

Can RT1015 write multiple GPIO at same time?

Regards

Ken

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,384 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ken Su

  If you check the GPIO register, it is not difficult to find, you can operate upto 32 GPIOs at the same time.

pastedImage_1.png

Because you can find the DR register can write each bit at the same time.

With it helps you!

     If you still have question about it, please kindly let me know.

 

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply