Hi giacomo mazzola ,
Do you test the official flexCAN example code in the RT1060 SDK? Just as the following SDK path code:
SDK_2.7.0_EVK-MIMXRT1060\boards\evkmimxrt1060\driver_examples\flexcan\interrupt_transfer
Whether this code can works OK on your side?
You can test it at first, then modify the code in the official SDK code to meet your own demand.
Please check it at first.
If you still have questions about it, please kindly let me know.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------