We are facing similar issue like this thread -> https://community.nxp.com/t5/i-MX-RT/i-MX-RT-eLCDIF-RGB-Mode-Use-Case/mp/981839
Configuration:
- 1024*600 display(RGB 565) - will convert it to RGB 888 later
- Using HS/VS mode instead of DE mode - As per RIVERDI display datasheet(attached)
- Started with sample example of RK043FN02H-CT display panel
Question -1: Are below setting correct?
godcks91_0-1682364951029.png
#define APP_HSW 1
#define APP_HFP 16
#define APP_HBP 160
#define APP_VSW 1
#define APP_VFP 1
#define APP_VBP 23
Question-2:
Below postDivider cannot be changed to 16 - We need Clock between 44.3 to 63. postDivider = 16 does not make any change in the clock. Is there any limitation to below equation? When I use loopDivider = 27 and postDivider = 8 - screen glows to white.
godcks91_1-1682365034838.png
When I do additional changes for clock - as per below snip - screen stopped glowing white but show few random lines. My frame buffer was not fully set as I did not use SDRAM for frame buffer.
godcks91_4-1682365640482.png
Question-3:
I have tried to use SDRAM(32MB) area for Non-Cachable region to store Frame buffer. Configured SDRAM to 27MB and allocate 5MB to Non-Cachable region. Is there any issue with this configuration? When I used SDRAM region like this - screen stopped glowing white - nothing on the screen - even some debug print stopped coming.
godcks91_2-1682365403890.png
godcks91_3-1682365446119.png
I even tried with above setting and stopping I & D cache like below
godcks91_5-1682365728745.png
Question - 4:
Is it okay to use -> #define FRAME_BUFFER_ALIGN 32 ? In example provided with imxrt1064 evk - it is 64.
Can someone please help us? We are trying to solve above issues for many days without any luck.
Thank you in advance!
- CS