Pin mux setting in LPSPI clocked interface.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Pin mux setting in LPSPI clocked interface.

跳至解决方案
1,604 次查看
takayuki_ishii
Contributor V

Hello community,

 

I try to use clocked interface of LPSPI.

In reference manual 47.3.3.3 Clocked Interface, it say that 

"For example, to configure PCS[0] to be always asserted, set PCSPOL[0] = 1, and don’t configure PCS[0] in the pin muxing."

In this sentence, "don’t configure PCS[0] in the pin muxing." mean that don't configure MUX_MODE bit in IOMUXC_SW_MUX_CTRL_PAD_xxxxx register to LPSPIx_PSCx. MUX_MODE bit must select some other pin like GPIOx_IOxx.

Is it correct?

 

Best regards,

Ishii.

 

 

0 项奖励
回复
1 解答
1,599 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it correct?
-- Yes, it's.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,600 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it correct?
-- Yes, it's.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,592 次查看
takayuki_ishii
Contributor V

Hello Jeremyzhou,

 

Thank you for your quick reply.

I will try to do it.

 

Best regards,

Ishii.

 

0 项奖励
回复