OTP Memory Usage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OTP Memory Usage

6,334 次查看
goodboy2024
Contributor II

RT1061 is used in our project.Recently we want to use the OTP function.I have a few questions as below.

1.All OTP space that can be used is shown in the OTP Memory Footprint?

2. Which part can be free used for our own software?It seems that some are used for special purpose

 

0 项奖励
回复
3 回复数

6,323 次查看
goodboy2024
Contributor II

Thanks for you reply.According to the datesheet,some area is for special use,for example,the rom patch.

I just want to use the area that doesnot affect other functions. Can you give some suggestion?

0 项奖励
回复

6,307 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
In the Fuse map, it doesn't demonstrate the area (0x830~0x870), in my opinion, this area likes the reserved area. Customers must not attempt to burn these.
If you want to store some data in the Fuse, you can program the value to the General Purpose fuse registers.
Hope it helps.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

6,326 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) All OTP space that can be used is shown in the OTP Memory Footprint?
-- No, the shadow registers don't reload to the value of all OTP space.
2) Which part can be free used for our own software?
-- It's able to manipulate all OTP space.
Hope this is clear
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复