Not able to debug MIMXRT1020-EVK board with P&E Multilink Universal FX
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hi,
I'm not able to debug MIMXRT1020-EVK board with P&E Multilink Universal FX. Tried with lowest debug frequency but result is same.
In same board Segger J-link works.
J25,J26,J27,J28 - All jumper is Open.
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
I'm working with EVK board since 1 month and I observed that if application is corrupt or some hard fault occur during debugging, thereafter I can not able to connect with any debugger. it gives connection error. I had tried with all the debugger On board DAP, Segger J-Link and PE Micro Universal FX also Delete the existing configuration of all compiler but not worked.
What I do in such condition I use segger debugger and J-Flash utility. Even in J-Flash it won't connect unless you manually hold RESET button for 1-2 seconds and simultaneously execute the connect command. Once it is connected successfully then erase the flash. After erasing the flash I can able to download the new application.
(Note: I have also added 2000 ms delay in Init steps but it won't work
This is very weird and time consuming process to run it again. I also face same problem in my custom board and it takes much time to develop my application.
Could you please help me to figure out the issue.
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello,
What version of MCUXpresso are you currently working with? Do you have the latest plugin from PEmicro? Try installing the latest plugin and see if you receive the same results.
Steve
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello,
How are you powering your board? I would suggest connecting via USB to J9 (USB OTG) and have Jumper J1 setting 3-4 as indicated in the user manual. Connecting through the Debug USB might interfere with P&E debugging products.
Steve
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
I checked Blue and Yellow led are ON.
It seems some reliability issue from PE Micro debugger, after many tries it start work when i power off the board and again power on then it again stop working but after USB cable reconnect and retried for few times it start work.
Is it generally happen with PE Micro? I'm new user of PE Micro.
I have not observed such problem with segger J-Link.
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello,
I have tried replicating this issue on my end with your project and a Multilink Universal FX but received no errors and was able to connect every time. I am using MCUXpresso 11.1.0 build 3150 with PEmicro plugin version 4.4.9.
I have attached a screenshot of my board to show jumper settings/power connections that I am using (also connecting to the 20-pin debug header).
If the set ups are the same and you are still having trouble, it may be the Multilink FX itself and I would suggest sending your unit in to PEmicro to see if that is the issue.
Steve


- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please ensure these resistors be soldered on the MIMXRT1020 board.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Do you say pull up resistor required for PE Micro debugger and not for others?
because Segger J-Link works without resistor?
If pull up resistor work for all debugger then why resistors are not placed on board?


- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hi ,
Thanks for your reply.
I'd like to eliminate the causes that are related to the board, in addition, I'd like to suggest you debug the MIMXRT1020 with the P&E Multilink Universal FX in other IDEs likes IAR, MDK, etc.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------


- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Thanks for your reply.
It seems a bit weird, however, I consider the issue is related to the P&E Multilink Universal FX, however, I don't have the P&E Multilink Universal FX on hand, so I'd like to suggest you ask for the support from the PEmicro's expert, they may have a new insight into the issue.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Not working with IAR V8.22.2.15996.
stuck at connection manager