NXP MIMXRT106 - PXP processing engine and emWin compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP MIMXRT106 - PXP processing engine and emWin compatibility

2,513件の閲覧回数
nandlol
Contributor I
Hello everyone, my name is Fernando.
I need to implement a GUI application on a LCD 4.3 inch TFT 480*272 pixels with LED Backlight and touch panel.
 
The MCU target is the NXP - MIMXRT1064CVJ5B with the built-in PXP (PXP pixel pipeline: 2D graphics and pixel/image) processing engine. The reference IDE is the µVision IDE - Keil.
 
I would like to know if the SEGGER emWin library fully supports this PXP processing engine or what are the incompatibly points, if necessary.
 
Thanks a lot,
Regards.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,500件の閲覧回数
jay_heng
NXP Employee
NXP Employee

You can refer to simple emWin demo in SDK:

\SDK_2_x_x_EVK-MIMXRT1064\boards\evkmimxrt1064\emwin_examples\emwin_gui_demo

The panel used in demo is https://www.nxp.com/part/RK043FN66HS-CTG#/

 

0 件の賞賛
返信

2,482件の閲覧回数
nandlol
Contributor I

thanks for the tip.

I looked into the example, but is not clear for me if the example takes advantage of the PXP peripheral or not.
I've more interesting to understand if the emWin library can be used exploiting the PXP accelerator.

Can you you link me some other examples or application notes that highlighted this point please?

Thanks

0 件の賞賛
返信

2,457件の閲覧回数
CarlosGarabito
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信