NXP MCU Boot Utility issue on IMXRT1060 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP MCU Boot Utility issue on IMXRT1060 EVK

3,549 Views
amitmehta
Contributor III

I am having an imxrt1060 EVK board and used NXP MCU Boot Utility to set JTAG interface to JTAG mode from SWD, but now I am not able to connect to board in normal mode using JTAG/SWD mode and also not able to set DAP_SEL bit to 0 for SWD mode

Labels (1)
7 Replies

3,088 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

1. Can you read out those eFuse data and paste here?

2. Can you use j-link Commander and try to connect cortex-M7 core?

0 Kudos
Reply

3,088 Views
amitmehta
Contributor III

Hi,

1. Below is a screenshot of eFuse data

pastedImage_1.png

pastedImage_2.png

2. J-Link Commander Screenshot

pastedImage_3.png

0 Kudos
Reply

3,088 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Please try to boot from eFuse.

pastedImage_1.jpg

Regards,

Jing

0 Kudos
Reply

3,088 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Amit,

What you write is in eFuse. It is an OTP memory. Only can write from 1 to 0.

The on board CMSIS-DAP firmware doesn't support JTAG. So, you have to use external debugger tool.

Regards,

Jing

3,088 Views
amitmehta
Contributor III

Hi Jing,

I have written 1 into DAP_SJC_SWD_SEL bit to configure JTAG interface into JTAG mode, after that I tried to connect using 20 pins onboard SEGGER header available on EVK, but I was not able to connect even after setting IAR Embedded workbench JTAG interface into from SWD to JTAG mode. even tried using J-Flash tool.

I am only able to communicate to the board using the NXP MCU Boot Utility.

0 Kudos
Reply

3,088 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

have you disconnect J47, j48, j49, j50?

Regards,

Jing

0 Kudos
Reply

3,088 Views
amitmehta
Contributor III

Hi,

Yes, Earlier before setting fuse bit I used to use the 20 pin segger for debugging by removing J47 and J48.

and even tried removing J47, j48, j49, j50 after setting fuse bit but no luck.

0 Kudos
Reply